Hi.
I found that when I quit after debugging the BEL example of the KW36 SDK, a debug error occurred from then on.
Among them, an error occurs after debugging the ble_fscibb example.
The error details are the same as the error encountered previously.
After debugging the example, I just clicked Terminate without executing any action, and the error occurred after that.
Why does this happen?
Hello,
Your FRDM might be in Low Power mode. Could you try to do a mass-erase? By using an "unlock kinetis" command in J-Link Commander, or a mass erase command through MCUXpresso, which works as well.
And the Low-Power mode can be disabled by setting the following macro (in the app_preinclude.h header file) to a 0, like so:
/* Enable/Disable PowerDown functionality in PwrLib */
#define cPWR_UsePowerDownMode 0
Hope this helps.
Regards,
Ricardo
Hello, Ricardo.
I am replying because the problem was not resolved after applying the method suggested as a solution.
First, I disabled low-power mode through macro modification.
Build has been completed.
Afterwards I tried "mass-erase".
'mass erase' was run in MCUXPresso, and the related settings were set as shown in the photo.
After setting it like this, I ran it, but an error occurred.
This is the error content.
An error message also appears in the console window.
As a result, 'mass erase' also doesn't seem to run due to a related error. What's the problem?
Regards,
SeokJin