AW-CM276MA-PUR build driver failed on x86 platform with Ubuntu 20.04 kernel 5.4 or 5.15.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

AW-CM276MA-PUR build driver failed on x86 platform with Ubuntu 20.04 kernel 5.4 or 5.15.

429件の閲覧回数
Andy_Hsieh
Contributor I

Hi Support,

Could you please let me know how can I build driver for AW-CM276MA-PUR on x86 platform with Ubuntu 20.04 kernel 5.4 or 5.15?

I would like to know how can I build driver successfully using the driver package on x86 platform with Ubuntu OS.

Do you have any document can be reference?

I tested locally with driver package named "FP92_PCIe_UART_123" but didn't work.

And also can you share me the latest driver package?

Andy_Hsieh_0-1671610496824.png

Looking forward to your assistance.

Best Regards,
Andy

0 件の賞賛
3 返答(返信)

416件の閲覧回数
Christine_Li
NXP TechSupport
NXP TechSupport

Hi, Andy, After download our Driver package, you can directly compile with "make build" command without any modification in Makefile.

It can be built successfully if you are using Ubuntu 20.04 Linux.

 

Please try this Driver: PCIE-WLAN-UART-BT-8997-U16-X86-16.92.21.p55.3-16.92.21.p55.3-MM5X16344.P3-MGPL

This driver code supports Linux kernel from 2.6.32 to 5.15.

You can find it on our website after log in.

Kindly remind: after log in, click "Design Resources",Choose "Software" and click "Secure Files" then click "Show all" button. image.png I also attach the download link below for your convenience.

I have tested it and made successfully on my local side(Ubuntu 20.04 on X86 platform)

https://www.nxp.com/webapp/sps/download/license.jsp?colCode=PCIE-WLAN.UART_BT_8997_U16.X86_MM5X16344...

 

For more build info details you can also see the README file in our driver package under WIFI-BT-U16-X86--MM5X17344.p3-MGPL/wlan_src directory after decompress it.

Above driver is not the latest one, but also new released this year(Sep 29, 2022).

The latest driver(PCIE-WLAN-UART-BT-8997-LNX_5_15_71-IMX8-16.92.21.p55.3-16.92.21.p55.3-MM5X16366.P5-MGPL ) download link is shown as below:

https://www.nxp.com/webapp/sps/download/license.jsp?colCode=PCIE-8997-LNX.5.15.71.p55.3-MM5X16366.P5...

 

Best regards,

Christine.

0 件の賞賛

363件の閲覧回数
Andy_Hsieh
Contributor I

Hi Christine,

Thank you for your response and information.

If we want to build driver on ARM system with OS Yocto or OpenWRT, do you have any SOP document or suggestion to guide us how to modify to make it work?

Thanks in advance.

0 件の賞賛

355件の閲覧回数
Christine_Li
NXP TechSupport
NXP TechSupport

HI, Andy,

Please refer to our user manual UM11675
How to Download and Build NXP Wi-Fi Drivers.

After login our website you can download it.

For ARM system, it is in part 6 Build the driver for ARM64 platforms on page 11.

 

Best regards,

Christine.

 

0 件の賞賛