88W9098 driver load parameter

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

88W9098 driver load parameter

593 Views
rahmanuh
Contributor III

Hello,

I am using 88W9098 chip and have some questions regarding the driver load parameters.

1. Why there are 2 blocks in mod_wifi_para.conf for PCIE9098? There are PCIE9098_0 and PCIE9098_1.

2. What is the max_vir_bss meaning and what it does in terms of feature? I haven't found the answer in the documentations.

Thanks.

Rahmanu

Labels (2)
0 Kudos
1 Reply

544 Views
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

Hi @rahmanuh,

Please accept my apologies for the late response.

You can refer to the wifi_mod_para.conf file, the blocks have a syntax as follows:

<card_type>[block_id]{

}

Multiple block ID's are used to support the same chipset with different module parameters.

The meaning of max_vir_bss is the number of virtual interfaces.

I hope this helps, Daniel.

0 Kudos