[chipset : NXP 88W8897]Channels Required for FCC DFS Testing (FCC Certified Vendor Requirement)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[chipset : NXP 88W8897]Channels Required for FCC DFS Testing (FCC Certified Vendor Requirement)

1,480 Views
cloudjo
Contributor I

chipset : NXP 88W8997

Channels required for FCC DFS test (required by FCC certified company)

1) For 20MHz bandwidth systems, use Channel
52, 56, 60, 64, 100, 104, 108, 112, 116, 120, 124, 128, 132, 136, 140, 144.
2) For 40MHz bandwidth systems, use Channel 54, 62, 102, 110, 118, 126, 134, 142.
3) For 80MHz bandwidth systems, use Channel 58, 106, 122, 138.
4) Test completed for Bandwidth 20MHz. The test is stopped because the corresponding channel of 40MHz/80MHz is not set.

Approved FCC-ID for NXP 88W8997: UAY-W8997-M1216

According to the FCC DFS TEST Report found with the above FCC ID (https://fcc.report/FCC-ID/UAY-W8997-M1216), the DFS test was performed on Channel 106 (5530MHz CF) as shown below.
1) Test-Report-DFS-pdf-3270029.pdf, page. 18 to 22

Is the 40MHz/80MHz channel supported?

0 Kudos
Reply
5 Replies

1,446 Views
estephania_mart
NXP TechSupport
NXP TechSupport

Hello,

 

Could you please help me with more details on which driver and software version are you using ?

0 Kudos
Reply

1,411 Views
cloudjo
Contributor I

Check the version
is this right?

 

wlan: version = PCIE8897-16.68.1.p88-C2615C110-GPL-(FP68)

0 Kudos
Reply

1,381 Views
estephania_mart
NXP TechSupport
NXP TechSupport

Hello,

 

Could you please help us check the internal information provided?

Regards

0 Kudos
Reply

1,343 Views
cloudjo
Contributor I

00471422 Case is already open.

0 Kudos
Reply

1,418 Views
cloudjo
Contributor I

How do I check the version?

0 Kudos
Reply