[88W8997] For getting SIG Certification.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[88W8997] For getting SIG Certification.

1,198 Views
waynejeong
Contributor II

Hello 

My customer have plan to get BT SIG certification with 88W8997.
I'm doing a DUT entry test using i.mx + AW-CM276MA-SUR to support them.
The following is the sequence I entered with fmapp command.

./fmapp ttymxc2 0x03 0x0003
./fmapp ttymxc2 0x03 0x0001 0x3f 0x27 0x00 0x00 0x00 0x00 0x00 0x00
./fmapp ttymxc2 0x03 0x0005 0x02 0x00 0x02
./fmapp ttymxc2 0x03 0x001A 0x03
./fmapp ttymxc2 0x06 0x0003

After that I could find the device with my phone. but when I try to connect to the device with my phone, a pop-up window appears asking me to enter a pin code.
Actually, I'm not sure if the device entered the DUT well.

i.mx board: MIMX8MQ
WIFI/BT module: AW-CM276MA-SUR
i.mx Android version: imx-android-11.0.0_2.4.0
Firmware name: sdiouart8997_combo_v4.bin
Firmware version: SD8997----16.92.10.p219.5-MM5X16266-GPL-(FP92)

1. My question is, is there a way to check if the device has successfully entered DUT mode?
2. May I get information how to get BT SIG certification on Android?
- BR/EDR
- BLE

Thank you.

Regards

Labels (1)
0 Kudos
Reply
1 Reply

1,182 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @waynejeong,

I can't share this information through this channel. I would contact you directly.

BR,

Alexis Andalon

0 Kudos
Reply