Vybrid VF6xx, Flex Timer, FAULT input

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Vybrid VF6xx, Flex Timer, FAULT input

跳至解决方案
1,665 次查看
axelrichter
Contributor I

Hello!

we want to use the Flextimer of the Vybrid as a H Bridge driver together with a FAULT input to set the output in a safe state.

In reference manual it is described how to initialize the FAULT input but not mentioned which input pin is used for it.

Is there a dedicated pin for that? So which pin is it?

Or can I use any other pin? How and where can I configure it in this case?

Best regards,

Axel Richter

标签 (2)
0 项奖励
1 解答
1,492 次查看
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

在原帖中查看解决方案

0 项奖励
3 回复数
1,493 次查看
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 项奖励
1,493 次查看
axelrichter
Contributor I

Any GPIO can be used, when configured as interrupt input. In the interrupt handling routine the desired fault bit in SRC_MISC1 has to be set.

0 项奖励
1,493 次查看
richard_stulens
NXP Employee
NXP Employee

That is indeed correct.

Regards,

Richard

0 项奖励