Is there a DDR3 stress test tool for the Vybrid processors?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Is there a DDR3 stress test tool for the Vybrid processors?

跳至解决方案
2,178 次查看
jamesherrera
Contributor II

Is there a DDR3 stress stress/calibration tool for the Vybrid processors like the i.MX6 tool?

标签 (5)
1 解答
1,086 次查看
naoumgitnik
Senior Contributor V

Yes, James, it is.

Please, review the Vybrid Hardware Development Guide (Rev.0) - initial (unofficial) draft. document; it describes the DDRv portion of the Processor Expert tool.

You will have to install the Processor Expert and Eclipse based Driver Suite (DS) v10.4, and then apply the "update 1" upgrading the DS to version v10.4.1, which includes the DDRv tool support for Vybrid.

(More information about DS here - http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=PE_DRIVER_SUITE.)

Regards, Naoum Gitnik.

在原帖中查看解决方案

0 项奖励
5 回复数
1,087 次查看
naoumgitnik
Senior Contributor V

Yes, James, it is.

Please, review the Vybrid Hardware Development Guide (Rev.0) - initial (unofficial) draft. document; it describes the DDRv portion of the Processor Expert tool.

You will have to install the Processor Expert and Eclipse based Driver Suite (DS) v10.4, and then apply the "update 1" upgrading the DS to version v10.4.1, which includes the DDRv tool support for Vybrid.

(More information about DS here - http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=PE_DRIVER_SUITE.)

Regards, Naoum Gitnik.

0 项奖励
1,086 次查看
antoniojenkins
Contributor II

Seems the DDRv for vybrid is not free?  Processor Expert is telling me I need a license.  This also seems to be tied to the Code Warrior suite....after some downgrading back to 10.4.1, the DDRv does seem to be doing some basic validation, but the tab named "validation" still says I need a license.  This does not give me a way to stress test, or calibrate.  So, I guess the original question stands.

1,086 次查看
jiri-b36968
NXP Employee
NXP Employee

Hello Antonio,

yes DDRv tool needs the license. Please talk to your NXP FAE (Field application engineer). There is 45 day temporary license available.

/Jiri

0 项奖励
1,086 次查看
antoniojenkins
Contributor II

The link to the dev guide above gives "Access to this place or content is restricted. If you think this is a mistake, please contact your administrator or the person who directed you here.".  How does one gain access to this document?

0 项奖励
1,086 次查看
naoumgitnik
Senior Contributor V

Dear Antonio,

Drafts are usually accessible by the company's FAEs only, but (tadaaam!) the guide is already published - http://cache.freescale.com/files/microcontrollers/doc/user_guide/VYBRIDHDUG.pdf?fasp=1.

Regards, Naoum Gitnik.