How to use nosigthresh of VYBRID RM of 61.6.27(VDEC_VSSGTH)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to use nosigthresh of VYBRID RM of 61.6.27(VDEC_VSSGTH)

ソリューションへジャンプ
1,145件の閲覧回数
takashitakahash
Contributor III

Hi,community

Our customer want to detection of signal or nosignal of NTSC imput.

Signal detection use register of VDEC_VIDMOD field descriptions of  bit "0" Have signal to set "1".

And detection level use VDEC_VSSGTH field description of "nosigthresh".

Question

Would please tell me what mean nosigthresh step by step valu.

If set to 0x001,Is this detect noise voltage? or noise period?

There are set to 0x101 is wlong. noise detection.

But set to 0x111 is no ploblem noise is no detect.

ラベル(1)
1 解決策
854件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

元の投稿で解決策を見る

0 件の賞賛
4 返答(返信)
855件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 件の賞賛
855件の閲覧回数
richard_stulens
NXP Employee
NXP Employee

Hi Takahashi-san,

We are still working on the details, but we believe the 3-bit field defines the threshold level for the input signal.

If the setting is 'n', then the threshold level is 2 ^(n+1). ex. if nosigthresh is set to 0b010, the threshold is 2^3 = 8.

Best regards,

Richard

855件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

richard_stulens​ do you have an update?

0 件の賞賛
855件の閲覧回数
richard_stulens
NXP Employee
NXP Employee

I think this is handled through the FAE's. This is the same project/issue as "VADC questions for NTSC input"

https://community.freescale.com/message/582045?et=watches.email.thread#582045

Regards,

Richard