How to use nosigthresh of VYBRID RM of 61.6.27(VDEC_VSSGTH)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to use nosigthresh of VYBRID RM of 61.6.27(VDEC_VSSGTH)

跳至解决方案
1,154 次查看
takashitakahash
Contributor III

Hi,community

Our customer want to detection of signal or nosignal of NTSC imput.

Signal detection use register of VDEC_VIDMOD field descriptions of  bit "0" Have signal to set "1".

And detection level use VDEC_VSSGTH field description of "nosigthresh".

Question

Would please tell me what mean nosigthresh step by step valu.

If set to 0x001,Is this detect noise voltage? or noise period?

There are set to 0x101 is wlong. noise detection.

But set to 0x111 is no ploblem noise is no detect.

标签 (1)
1 解答
863 次查看
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

在原帖中查看解决方案

0 项奖励
4 回复数
864 次查看
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 项奖励
864 次查看
richard_stulens
NXP Employee
NXP Employee

Hi Takahashi-san,

We are still working on the details, but we believe the 3-bit field defines the threshold level for the input signal.

If the setting is 'n', then the threshold level is 2 ^(n+1). ex. if nosigthresh is set to 0b010, the threshold is 2^3 = 8.

Best regards,

Richard

864 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

richard_stulens​ do you have an update?

0 项奖励
864 次查看
richard_stulens
NXP Employee
NXP Employee

I think this is handled through the FAE's. This is the same project/issue as "VADC questions for NTSC input"

https://community.freescale.com/message/582045?et=watches.email.thread#582045

Regards,

Richard