Hello,
I would like to run a simple application that uses hardware semaphores on phyCore board (Vybrid PVF65GS10CMK40 test rev.). I have a problem with
modifying CP1INE register. Whatever I do, any write access to this register causes Hard Fault.
This is a code sample:
#define GATE (*(volatile unsigned char*)(0x4001D000))
#define CPINE (*(volatile unsigned short*)(0x4001D048))
int main()
{
SystemInit(); // Sets vector table and enables all peripheral clocks excepting GPU
CPINE = 0x1000;
GATE = 2;
while(1)
{
}
}
Solved! Go to Solution.
Hi Matthew,
I had the same problem and this was the solution:
The Reference Manual states that the offset to the SEMA4_CP1INE Register is 48, but when i take a look at the SEMA4_MemMap struct in the "MVF50GS10MK50.h" file the offset seems to be 50:
- /** SEMA4 - Peripheral register structure */
- typedef struct SEMA4_MemMap {
- uint8_t GATE[16];
- uint8_t RESERVED_0[50]; /* 48 */
- uint16_t CP0INE; /**< Semaphores Processor n IRQ Notification Enable, offset: 0x40 */
- uint8_t RESERVED_1[6];
- uint16_t CP1INE; /**< Semaphores Processor n IRQ Notification Enable, offset: 0x48 */
- uint8_t RESERVED_2[54];
- uint16_t CP0NTF; /**< Semaphores Processor n IRQ Notification, offset: 0x80 */
- uint8_t RESERVED_3[6];
- uint16_t CP1NTF; /**< Semaphores Processor n IRQ Notification, offset: 0x88 */
- uint8_t RESERVED_4[118];
- uint16_t RSTGT; /**< Semaphores (Secure) Reset Gate n, offset: 0x100 */
- uint8_t RESERVED_5[2];
- uint16_t RSTNTF; /**< Semaphores (Secure) Reset IRQ Notification, offset: 0x104 */
- } volatile *SEMA4_MemMapPtr;
maybe this helps.
Best Regards
Simon
Hi Matthew,
I had the same problem and this was the solution:
The Reference Manual states that the offset to the SEMA4_CP1INE Register is 48, but when i take a look at the SEMA4_MemMap struct in the "MVF50GS10MK50.h" file the offset seems to be 50:
- /** SEMA4 - Peripheral register structure */
- typedef struct SEMA4_MemMap {
- uint8_t GATE[16];
- uint8_t RESERVED_0[50]; /* 48 */
- uint16_t CP0INE; /**< Semaphores Processor n IRQ Notification Enable, offset: 0x40 */
- uint8_t RESERVED_1[6];
- uint16_t CP1INE; /**< Semaphores Processor n IRQ Notification Enable, offset: 0x48 */
- uint8_t RESERVED_2[54];
- uint16_t CP0NTF; /**< Semaphores Processor n IRQ Notification, offset: 0x80 */
- uint8_t RESERVED_3[6];
- uint16_t CP1NTF; /**< Semaphores Processor n IRQ Notification, offset: 0x88 */
- uint8_t RESERVED_4[118];
- uint16_t RSTGT; /**< Semaphores (Secure) Reset Gate n, offset: 0x100 */
- uint8_t RESERVED_5[2];
- uint16_t RSTNTF; /**< Semaphores (Secure) Reset IRQ Notification, offset: 0x104 */
- } volatile *SEMA4_MemMapPtr;
maybe this helps.
Best Regards
Simon
Hi Simon,
It seems to work now! Thanks for help.
Best regards
Matthew
I am sorry, out of habit, I have pressed Ctrl+S and that caused sending my question :smileyhappy: before I finished writing it. More details here:
This is an excerpt from disassembly. As you can see I use 16-bit access to write CP1INE. Read access does not cause Hard Fault.
0x3F00037C : LDR r0,[pc,#32] ; [0x3F0003A0] = 0x4001D000
0x3F00037E : MOV r1,#0x1000
0x3F000382 : STRH r1,[r0,#0x48]
0x3F000386 : MOVS r1,#2
0x3F000388 : STRB r1,[r0,#0]
Besides on HardFault CFSR is set to 0x00000400 (IMPRECISERR).
Did I miss something? May it be a silicon bug (eventually this is test PF revision)?
Thanks in advance.
Hi Matthew,
I have seen that the most common reason that generates a hard fault is trying to write to a module whose clock gate is off.
Make sure that the correct CCM_CCPGRn bits and register is set for the SEMA4 module.
I hope that helps,
Alejandro
Hi Alejandro,
Thanks for reply. I was able to lock the gates by writing the core number + 1 to GATE registers so SEMA4 module clock was on. I have not modified CCPGR bits as they are set after reset by default.
The Simon's hint was good direction to solve the problem.
Best regards,
Matthew