CAN FD and Partial Networking

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CAN FD and Partial Networking

CAN FD and Partial Networking

Provide an overview of the protocol and implementation of CAN FD in system architectures, including the use of partial networking in relation to the deployment of CAN FD.

附件
评论

If CAN FD communication is exposed to a CAN node, the CAN node willsee the CAN FD frame as an error and block the communication, thereby rendering the network useless. By using original CAN protocol on the CAN FD nodes all advantages of CAN FD are lost. prepaidgiftbalance

I am using i.MXRTOS1170 EVKB. I am using sample project "evkbmimxrt1170_canfd_interrupt_transfer_cm7" but it is not working the way it should I am getting garbage data from transmitter. Any help. I configured CAN3 and LPUART1 no warnings or errors.

It is failing below 

mdkhaledibnhassan_0-1707219128390.png

 

100% 有帮助 (1/1)
版本历史
最后更新:
‎10-22-2018 04:07 PM
更新人: