CAN FD and Partial Networking

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CAN FD and Partial Networking

CAN FD and Partial Networking

Provide an overview of the protocol and implementation of CAN FD in system architectures, including the use of partial networking in relation to the deployment of CAN FD.

添付
コメント

If CAN FD communication is exposed to a CAN node, the CAN node willsee the CAN FD frame as an error and block the communication, thereby rendering the network useless. By using original CAN protocol on the CAN FD nodes all advantages of CAN FD are lost. prepaidgiftbalance

I am using i.MXRTOS1170 EVKB. I am using sample project "evkbmimxrt1170_canfd_interrupt_transfer_cm7" but it is not working the way it should I am getting garbage data from transmitter. Any help. I configured CAN3 and LPUART1 no warnings or errors.

It is failing below 

mdkhaledibnhassan_0-1707219128390.png

 

100%が役に立ったと言っています (1/1)
バージョン履歴
最終更新日:
‎10-22-2018 04:07 PM
更新者: