T2080 PCIe polarity reversal

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T2080 PCIe polarity reversal

ソリューションへジャンプ
842件の閲覧回数
tomsaluzzo
Contributor III

Please confirm T2080 supports PCIe polarity reversal on the RX port as per the PCIe spec. I couldn't find it documented in the T2080 documentation.

ラベル(1)
0 件の賞賛
1 解決策
691件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

元の投稿で解決策を見る

0 件の賞賛
2 返答(返信)
692件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 件の賞賛
693件の閲覧回数
Bulat
NXP Employee
NXP Employee

The T2080 PCI Express interface is compatible with the PCI Express Base Specification, Revision 3.0, this assumes that it supports all features from the specifications.

0 件の賞賛