Regarding fsl sdk v2.0 on t2080qds with hypervisor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Regarding fsl sdk v2.0 on t2080qds with hypervisor

746 Views
ronakadesai
Contributor II


Hi,

I am using fsl sdk v2.0's kernel, devicetree and hypervisor on t2080qds devkit. Everything is in 64 bit mode. But, I am getting following crash when I boot hypervisor. Without using the hypervisor my kernel boots without any error.

Kernel config : corenet64_fmanv3h_smp (Default from kernel)

Kernel Device tree : t2080qds.dts (Default from kernel)

Hypervisor config : t2080qds/RR_PNNPPH_66_16/hv-2p-lnx-lnx (From hv-config.git)

WARNING: adjusting available memory to 30000000

## Booting kernel from Legacy Image at ec700000 ...

   Image Name: 

   Image Type:   PowerPC Linux Kernel Image (uncompressed)

   Data Size:    551040 Bytes = 538.1 KiB

   Load Address: 00000000

   Entry Point:  00000000

   Verifying Checksum ... OK

## Flattened Device Tree blob at ec800000

   Booting using the fdt blob at 0xec800000

   Loading Kernel Image ... OK

   Loading Device Tree to 03fe3000, end 03fffb28 ... OK

[0] =======================================

[0] Freescale Hypervisor 1.3-012 ppc64

[0] Hypervisor command line: config-addr=0xfec900000 console=ttyS0,115200

[0] malloc_init: using 12357 KiB at 0x7f2e3af0 - 0x7fef4fff

[0] malloc_init: using 1060 KiB at 0x7fef6000 - 0x7fffefff

[0] dt_read_aliases: Alias pci2 points to non-existent /pcie@ffe260000

[0] assign_callback: device buffer-pool@7 in buffer-pool@7 not found

[0] assign_callback: device buffer-pool@8 in buffer-pool@8 not found

[0] assign_callback: device buffer-pool@9 in buffer-pool@9 not found

[0] assign_callback: device buffer-pool@16 in buffer-pool@16 not found

[0] assign_callback: device buffer-pool@17 in buffer-pool@17 not found

[0] assign_callback: device pci2 in pci2 not found

[0] assign_callback: device rman in rman not found

[0] assign_callback: device /fsl,dpaa/ethernet@16 in dpa-ethernet@16 not found

[0] assign_callback: device /fsl,dpaa/dpa-fman0-oh@1 in dpa-fman0-oh@1 not found

HV>                                                                                                                                                                                                              [0] unexpected trap in hypervisor

[0] data tlb miss

[0] NIP 0x004093c8 MSR 0x80001002 LR 0x0040a6c4 ESR 0x00000000 EXC 13

CTR 0x0040a480 CR 0x28424022 XER 0x20000000 DEAR 0x00000000 PIR 0

Prev trap level 0

r00 0x004309c0  r01 0x006e3190  r02 0x0048e880  r03 0x0048ffc0

r04 0x00000005  r05 0x00000004  r06 0x0000003f  r07 0x00000008

r08 0x004594a0  r09 0x00000000  r10 0x00007000  r11 0x00000000

r12 0x48424022  r13 0x00479b40  r14 0x0045e5d0  r15 0x0045f220

r16 0x7f30b450  r17 0x80029002  r18 0x14318000  r19 0x00000002

r20 0x7f979510  r21 0x0045cc90  r22 0x00000000  r23 0x00001000

r24 0x0048f8b8  r25 0x0048ffc0  r26 0x004888b8  r27 0x80001002

r28 0x00008000  r29 0x0048ffc0  r30 0x7f326f10  r31 0x00000100

[0] sp 6e3190 6e3250 12 6e3240 1000000deadbeef

[0] Traceback: 0x7f2e3e9c 0x48424022006824c0 0x0045f21c 0x4842402200685abc 0x284220440047e87c 0x220020820047325c

0x0045da24 0x24002023fffffffc 0xfffffffffffffffc

Labels (1)
0 Kudos
1 Reply

465 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Ronak Desai,

According to the log, it seems that you didn't deploy images and configure Hypervisor command line correctly, please refer to the following.

uImage(linux):0xE8020000-0xE87FFFFF

fsl-image-core-t2080qds.ext2.gz.u-boot(rootfs): 0xE9300000-0xEBEFFFFF

hv.uImage: 0xE8700000-0xE87FFFFF

uImage-t2080qds.dtb(linux dtb):0xE8800000-0xE92FFFFF

hv-2p-lnx-lnx.dtb(hv dtb): 0xE8900000-0xE89FFFFF

=>setenv bootargs config-addr=0xfe8900000 console=ttyS0,115200

=>setenv bootcmd 'bootm 0xfe8700000 - 0xfe8800000'


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos