Marvel Ethernet Switch connection issue with T1022 Processor

取消
显示结果 
搜索替代 
您的意思是: 
已解决

Marvel Ethernet Switch connection issue with T1022 Processor

跳至解决方案
585 次查看
hemwant
Contributor IV

We are having T1022 processor customized board , the SERDES configuration used in the RCW is 0x40.  The EC1 is connected to ethernet marvel switch (88E6320) port 5 with RGMII interface. Now we have initialised marvel switch port 5 with following configuration - speed 1G , full duplex autoneg off with forced link up.  The processor is able to receive ICMP packets from switch but is not sending the ICMP reply. All delay combination of rgmii have been tried in device tree as well as in switch.

I am attaching device tree which i am using for the above purpose.

标签 (1)
0 项奖励
1 解答
536 次查看
hemwant
Contributor IV

In my case , by mistake one bridge was working on the above ethernet interface. After removing the above bridge configuration the issue was solved.

在原帖中查看解决方案

0 项奖励
1 回复
537 次查看
hemwant
Contributor IV

In my case , by mistake one bridge was working on the above ethernet interface. After removing the above bridge configuration the issue was solved.

0 项奖励