Marvel Ethernet Switch connection issue with T1022 Processor

キャンセル
次の結果を表示 
次の代わりに検索 
もしかして: 

Marvel Ethernet Switch connection issue with T1022 Processor

ソリューションへジャンプ
606件の閲覧回数
hemwant
Contributor IV

We are having T1022 processor customized board , the SERDES configuration used in the RCW is 0x40.  The EC1 is connected to ethernet marvel switch (88E6320) port 5 with RGMII interface. Now we have initialised marvel switch port 5 with following configuration - speed 1G , full duplex autoneg off with forced link up.  The processor is able to receive ICMP packets from switch but is not sending the ICMP reply. All delay combination of rgmii have been tried in device tree as well as in switch.

I am attaching device tree which i am using for the above purpose.

ラベル(1)
0 件の賞賛
1 解決策
557件の閲覧回数
hemwant
Contributor IV

In my case , by mistake one bridge was working on the above ethernet interface. After removing the above bridge configuration the issue was solved.

元の投稿で解決策を見る

0 件の賞賛
1 返信
558件の閲覧回数
hemwant
Contributor IV

In my case , by mistake one bridge was working on the above ethernet interface. After removing the above bridge configuration the issue was solved.

0 件の賞賛