Media Compatibility of MPXH6300A/MPXx6250A/MPXH6400A pressure sensors

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Media Compatibility of MPXH6300A/MPXx6250A/MPXH6400A pressure sensors

560 Views
medengi
Contributor I

Hello,


I would like to ask regarding media compatibility of your sensor series which use fluorosilicone gel and media-compatible gel. Specifically, MPXH6300A/MPXx6250A/MPXH6400A. 

Is there a list of liquids which are compatible with each of fluorosilicone/media-compatible gels?
Is performance affected over long periods of direct contact with liquids? 

Specifially, I'd like to know if silicone oil is a suitable liquid to use in combination with these sensors.

Best Regards,

Dmitri 

0 Kudos
2 Replies

434 Views
medengi
Contributor I

Hello Tomas,


I have previously read the document you link to, and it provides some useful information. 
However, it is slightly unclear what the results in the table say: 

For example: In the second column under "media resistant gel" I see both "Tested" and "Okay". Does this mean that "Tested" is okay or not okay? 


Also, looking at the table, no conclusions can be drawn on the long-term characteristics using the different gels. Could you please provide more information on these topics? 

Best Regards,

Dmitri 

0 Kudos

434 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Dmitri,

I would recommend taking a closer look at our AN3728 which deals with the media compatibility of NXP IPS with both a Fluorosilicone and an improved Media Resistant gel.

Best regards,

Tomas

0 Kudos