Measure vacuum pressure via MPXV6115V

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Measure vacuum pressure via MPXV6115V

跳至解决方案
1,886 次查看
LORDSUN1
Contributor I

When I used the Arduino board and the MPXV6115V sensor to measure the vacuum pressure, the output from the Vout pin shows the value around 900, which should be 1023 (due to the ADC function of the Arduino board).

I am not sure why this happens. Is it normal for the vacuum pressure sensor?

0 项奖励
回复
1 解答
1,878 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Xiyang,

 

Which Arduino board are you actually using and what is the voltage (in Volts) on the Vout pin? You should see something around 4.6V with no pressure applied and 5.0V supply voltage:

 

Capture.JPG

 

Best regards,

Tomas

   

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,879 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Xiyang,

 

Which Arduino board are you actually using and what is the voltage (in Volts) on the Vout pin? You should see something around 4.6V with no pressure applied and 5.0V supply voltage:

 

Capture.JPG

 

Best regards,

Tomas

   

0 项奖励
回复
1,872 次查看
LORDSUN1
Contributor I

Thanks for your kind notification.

Yes, you're right. The arduino board I used is the Arduino Mega 2560, the output from the pressure sensor is around 900, due to the Analog-digital-conversion, thus the output voltage should be 900/1023*5 V, around 4.5V.

0 项奖励
回复