Measure vacuum pressure via MPXV6115V

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Measure vacuum pressure via MPXV6115V

ソリューションへジャンプ
1,889件の閲覧回数
LORDSUN1
Contributor I

When I used the Arduino board and the MPXV6115V sensor to measure the vacuum pressure, the output from the Vout pin shows the value around 900, which should be 1023 (due to the ADC function of the Arduino board).

I am not sure why this happens. Is it normal for the vacuum pressure sensor?

0 件の賞賛
返信
1 解決策
1,881件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Xiyang,

 

Which Arduino board are you actually using and what is the voltage (in Volts) on the Vout pin? You should see something around 4.6V with no pressure applied and 5.0V supply voltage:

 

Capture.JPG

 

Best regards,

Tomas

   

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,882件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Xiyang,

 

Which Arduino board are you actually using and what is the voltage (in Volts) on the Vout pin? You should see something around 4.6V with no pressure applied and 5.0V supply voltage:

 

Capture.JPG

 

Best regards,

Tomas

   

0 件の賞賛
返信
1,875件の閲覧回数
LORDSUN1
Contributor I

Thanks for your kind notification.

Yes, you're right. The arduino board I used is the Arduino Mega 2560, the output from the pressure sensor is around 900, due to the Analog-digital-conversion, thus the output voltage should be 900/1023*5 V, around 4.5V.

0 件の賞賛
返信