Accelerometer: MMA865x Breakout Board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Accelerometer: MMA865x Breakout Board

Accelerometer: MMA865x Breakout Board

Hi,

The MMA865x, 3-axis, 10-bit/12-bit accelerometer that has industry leading performance in a small 2 x 2 x 1 mm DFN package. This accelerometer is packed with embedded functions that include flexible user-programmable options and two configurable interrupt pins. Overall power savings is achieved through inertial wake-up interrupt signals that monitor events and remain in a low-power mode during periods of inactivity.

Here is a Render of the MMA865x Breakout- Board downloaded from OSH park:

PCB Render.png

Layout Design for this board:

Layout Render.png

In the attachments section, you can find the Schematic Source File (SCH), Schematic PDF File, Layout Source File (BRD), Gerber Files (GTL, GBL, GTS, GBS, GTO, GBO, GKO, XLN) and BOM files.

If you're interested in more designs like this breakout board for other sensors, please go to Freescale Sensors Breakout Boards Designs – HOME

ラベル(1)
添付
評価なし
バージョン履歴
最終更新日:
‎01-21-2015 03:42 PM
更新者: