S32k116 FMEDA FIT rate distribution

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32k116 FMEDA FIT rate distribution

280 次查看
Sushmitha_V
Contributor I

Sushmitha_V_0-1723033416923.png

The FIT rate distribution is not provided for any of the Failure modes for any component could that details be provided.

0 项奖励
1 回复

178 次查看
Yashwant_Singh
NXP Employee
NXP Employee

Hello,

The failure mode distributions are actually mentioned the failure modes column. The failuremmo

Stuck-at for data and addresses and control interface, lines and logic (70%)
Stuck-at open for data and addresses and control interface, lines and logic (5%)
Open or hugh impedance for data and address and control interface, lines and logic (20%)
Short circuit between data and address and control intrefaces, lines and logic (5%)
 
However, the FMEDA considers the coverage of the safety mechanism over the raw dangerous failure rate of the component itself instead of the dangerous failure rate corresponding to individual failure modes to get the λSPFRF.
This is because the same safety mechanism and DC coverage is considered for all failure modes.
 
Hoping this helps.
 
Thanks!
-Yashwant
 
0 项奖励