S32K1xx - SM_075
- 新着としてマーク
- ブックマーク
- 購読
- ミュート
- RSS フィードを購読する
- ハイライト
- 印刷
- 不適切なコンテンツを報告
Hello,
Questions on this Safety Manual Assumption:
1. Who normally provides the FT-COM layer? Is it Vector?
2. How does a customer confirm that they meet this assumption? What would it look like?
3. Is this relevant only for Fault Tolerant CAN or any CAN bus including CAN-FD?
Thank you,
John
- 新着としてマーク
- ブックマーク
- 購読
- ミュート
- RSS フィードを購読する
- ハイライト
- 印刷
- 不適切なコンテンツを報告
Hello John,
Please find some answers below:
1. The FT-COM layer means Fault-Tolerant Communication Layer which is a set of application level software components used to detect and recover from faults that are not handled by hardware. This FT-COM layer is created by the customers or can be provided by several vendors. Refer to SM_051 for more details.
2. The [SM_075] means that as the FlexCAN module and CLKOUT feature can use the SOSC as clock source (coming from an external component), any clock failure must be detected by the FT-COM layer. When you are able to detect the failures of the SOSC in the FT-COM layer, the assumption is fulfilled.
3. It is applicable for all CAN protocols including CAN-FD.
Hope these answer the below query.
Kind Regards,
Avni