216468 - REG_PROT query

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

216468 - REG_PROT query

106 Views
RandyKrakora
NXP Employee
NXP Employee

Customer is Ford.

 

AOU 216468 and 25593:

to fulfill static configuration registers check via : REG_PROT, XRDC and MMU.

we have way of fulfilling static configuration registers check of MSCM static registers by periodic interrupt monitoring .

Is it sufficient to fulfill the given AoUs or do we need to implement REG_PROT for individual registers as well.

 

if yes, could you please help us with the registers which needs to be protected/verified by REG_PROT.

Note: As discussed, only MSCM configuration registers are leading to single point failures.

 

-Randy Krakora

Labels (1)
0 Kudos
1 Reply

78 Views
antoinedubois
NXP Employee
NXP Employee

Hi Randy,

Static configuration register check is sufficient if done periodically within FTTI. This solution will detect failure.

REG PROT can be used to prevent the failure from happening, what they are going is actually what we recommend for newer device.

Antoine

0 Kudos