Synchronous Abort Issue S32V

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Synchronous Abort Issue S32V

5,432 Views
hfahema
Contributor I

Hello Experts!

I am receiving this error message here when trying to boot an S32V234 from an SD card.

 

U-Boot 2016.01+g4627170 (May 22 2019 - 12:48:54 -0700)

CPU: NXP S32V234 V2.0 at 1000 MHz
Reset cause: Software Functional reset
Board: s32v234bbmini
I2C: ready
DRAM: "Synchronous Abort" handler, esr 0x96000010
ELR: 3e828200
LR: 3e84816c
x0 : 000000007fd7af68 x1 : 000000003e856832
x2 : 0000000080000000 x3 : 000000003e8281ec
x4 : 000000007fd7b000 x5 : 0000000000000013
x6 : 0000000000000098 x7 : 0000000020000000
x8 : 00000000fffff7ff x9 : 000000000000000c
x10: 00000000feeff7ff x11: 000000003ebdfa8d
x12: 00000000ffffffff x13: 00000000ffffffff
x14: 0000000080000000 x15: 0000000080010000
x16: 000000003e822530 x17: 2114214011001432
x18: 000000003ebdfca0 x19: 000000003e85e0f0
x20: 000000003e85dfe8 x21: 0000000000000000
x22: 042401a8bf30080e x23: ff980013008de800
x24: 0c01310935d14c10 x25: 3002101258802340
x26: 45098e49014f1628 x27: b00005020a90b602
x28: 498aa85c99a10024 x29: 000000003ebdfc50

Resetting CPU ...

resetting ...


U-Boot 2016.01+g4627170 (May 22 2019 - 12:48:54 -0700)

CPU: NXP S32V234 V2.0 at 1000 MHz
Reset cause: Software Functional reset
Board: s32v234bbmini
I2C: ready
DRAM: "Synchronous Abort" handler, esr 0x96000010
ELR: 3e828200
LR: 3e84816c
x0 : 000000007fd6af68 x1 : 000000003e856832
x2 : 0000000080000000 x3 : 000000003e8281ec
x4 : 000000007fd6b000 x5 : 0000000000000013
x6 : 0000000000000098 x7 : 0000000020000000
x8 : 00000000fffffffd x9 : 000000000000000c
x10: 00000000ffeffffd x11: 000000003ebdfa8d
x12: 00000000ffffffff x13: 00000000ffffffff
x14: 0000000080000000 x15: 0000000080010000
x16: 000000003e822530 x17: 2114214011001432
x18: 000000003ebdfca0 x19: 000000003e85e0f0
x20: 000000003e85dfe8 x21: 0000000000000000
x22: 042401a8bf30080e x23: ff980013008de800
x24: 0c01310935d14c10 x25: 3002101258802340
x26: 45098e49014f1628 x27: b00005020a90b602
x28: 498aa85c99a10024 x29: 000000003ebdfc50

Resetting CPU ...

 

This error continues repeating indefinitely. I am asking for help from the NXP community about how to interpret this error and also possible reasons for this error. I believe this error can either be coming from a corrupted SD card or compromised communication to the DDR3 chips.

 

I can provide more information upon request. Thank you for the help!

Tags (1)
0 Kudos
Reply
2 Replies

5,025 Views
KushalShahNXP
NXP Employee
NXP Employee

Hi,

 

We have stopped supporting this community. But we still support S32V2 questions using our ticketing system.

Please create the request at www.nxp.com/support using Support Requests option. Our experts will help you.

 

Thank you for understanding.

 

Regards,

Kushal

0 Kudos
Reply

5,025 Views
evalese
NXP TechSupport
NXP TechSupport
Comment added on behalf of customer (requested by chat):
Hussein Fahema

Ok I would like to add

I will purchase a debugger tool soon and I need some guidance on which one to select. Also, a bit of help started with it would be greatly appreciated. I need to know which registers to read for the data on the reset and how to read them.

0 Kudos
Reply