use internal reference voltage for ADC S32K14X

取消
显示结果 
搜索替代 
您的意思是: 

use internal reference voltage for ADC S32K14X

197 次查看
naderkhamess
Contributor III

Hello there,

We are working with MCU S32K14X ADC and we were wondering, is there internally generated reference voltage can be used for vref in the ADC instead of using external vref ? the issue is the external supply is not stable and we need to have stable vref provided internally for the ADC if possible.

if feasible, what are the internal reference voltage options?

Thanks.

Best regards,

Nader Khamess

标记 (3)
0 项奖励
1 回复

178 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Nader Khamess,

There is no internal reference voltage can be used as ADC VREF.

43.6 ADC Reference Options.png

There is 1V bandgap, but it's ADC input not vref. 

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励