the installation of S32 DS 3.2 falied

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

the installation of S32 DS 3.2 falied

741 Views
LIUOP
Contributor I

Hi.I have met a problem when installing S32DS 3.2.I have used the activation code to choose online activation at the first time but failed.Then,I uninstalled it and reinstalled it and the installation rolled back.The problems are listed in the pictures and logs in detail.Thanks!(I have also tried v3.3 and v3.4 ,falied)

0 Kudos
Reply
8 Replies

677 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Do you run the installation as ADMIN?

Otherwise it wont work. Also check your firewall settings.

Eventually ask your IT department for help with installation, as this seems to be linked to your personal PC settings.

Best regards,

Peter

0 Kudos
Reply

661 Views
LIUOP
Contributor I
Could you tell how I should modify PC settings according to my log?
Best regards,Liu
0 Kudos
Reply

659 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Please get in touch with your IT support / admin.

That you need to execute installation as an Admin.

I can hardly help you with that as I do not know your PC system.

Are you executing it as admin? Otherwise it wont work under Windows system.

Best regards,

Peter

0 Kudos
Reply

656 Views
LIUOP
Contributor I
hello,I have executed installation as an Admin but still failed.Could you tell me how to get in touch with IT suppot?
0 Kudos
Reply

620 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

I was talking to our flexera expert.

It looks like some incompatibility at your side.

Do you use windows 11 ? Or could you specify the system you are using?

Best regards,

Peter

0 Kudos
Reply

622 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

I checked your account and it looks, that you successfully installed and activated S32DS v3.5 on Jul 20. If it is new installation - the roll back is after you enter the activation code or in which point? 

Did you tried offline activation? 

0 Kudos
Reply

465 Views
LIUOP
Contributor I
yes
0 Kudos
Reply

708 Views
LIUOP
Contributor I

help,thanks!

0 Kudos
Reply