s32k344 CAN bus sample code hard fault issue.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

s32k344 CAN bus sample code hard fault issue.

跳至解决方案
1,661 次查看
StephenYeh
Contributor III

Hi Sir

I will import the sample code s32k344 CAN bus sample code.

When enter debug mode, and the code will hang on startup.cm7.s?

My SDK version is the D2203.

I also chech the FlexCAN_ip, also hang on the same condition.

Would you share us the CAN sample code for S32K312 and S32K344?

 

StephenYeh_0-1653904904361.png

 

 

StephenYeh_2-1653905070431.png

 

标记 (1)
0 项奖励
回复
1 解答
1,641 次查看
namnguyenviet
NXP Employee
NXP Employee

Hello,

As your capture, the code is staying at end_of_eunit_test, which means the example has finished. It's a normal behavior and also proved that there was no problem with the example.

Best Regards,

Nam

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,631 次查看
StephenYeh
Contributor III

Hi Nam

Thanks.

Would you share the CAN RX FIFO mode sample code?

0 项奖励
回复
1,642 次查看
namnguyenviet
NXP Employee
NXP Employee

Hello,

As your capture, the code is staying at end_of_eunit_test, which means the example has finished. It's a normal behavior and also proved that there was no problem with the example.

Best Regards,

Nam

0 项奖励
回复