s32k144 FREETOS with lpspi is stuck in vPortRaiseBASEPRI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

s32k144 FREETOS with lpspi is stuck in vPortRaiseBASEPRI

1,616 Views
sandeepsandeepk
Contributor II

i am doing project with the two spi on as slave and other as a master and it workis without a freertos but, with freertos it stuck in vPortRaiseBASEPRI plesae give me a solution for this.

I think it is with the interrupt priority between the peripheral isr like SPI and freeRTOS some settings need to be made for this please help me for this setting.

Labels (1)
0 Kudos
1 Reply

1,536 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hello Sandeep,

In the following thread there's a previous question that could match the one that you have:

https://community.nxp.com/message/1285431 

Best Regards,

Alexis Andalon

0 Kudos