s32k118 Keep sending I2C Data when Flash operation is doing.(read/write)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

s32k118 Keep sending I2C Data when Flash operation is doing.(read/write)

跳至解决方案
585 次查看
Yooyi
Contributor I

I have a Host that keep sending I2C data, when I open S32K118 MCU and do flash operation.
I2C Bus abnormal condition has occurred which like picture. I don't know why I2C bus
 is affected by Flash operation. 

0 项奖励
回复
1 解答
516 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@Yooyi

1. You can do some handshake operations, such as using a GPIO port to indicate the status of the Slave, and the Master can suspend sending until the Slave resumes normal operation.


2. Or the Master checks the communication failure and then suspends sending

在原帖中查看解决方案

3 回复数
544 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@Yooyi

Because in the I2C protocol, although the clock comes from the Master node, the Slave node may only passively receives the clock from the Master, but the Slave can hold or release the clock from the Master when working, so the Clock status is not completely determined by the Master.
When you burn the program to the MCU, Slave node cannot work normally, it may always hold or release the clock, resulting in this error condition.

534 次查看
Yooyi
Contributor I
Once an abnormal wave pattern occurs, the I2C is likely to be damaged, causing the I2C fail to communicate normally. Is there any method which can solve it effective this problem ?
0 项奖励
回复
517 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@Yooyi

1. You can do some handshake operations, such as using a GPIO port to indicate the status of the Slave, and the Master can suspend sending until the Slave resumes normal operation.


2. Or the Master checks the communication failure and then suspends sending