s32k118无法烧录程序,JLINK找不到目标芯片。

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

s32k118无法烧录程序,JLINK找不到目标芯片。

Jump to solution
5,206 Views
Sally_Wang
Contributor I

 使用S32DS进行硬件设计,连接自研的电路板,debug出现鼓掌无法识别到芯片。后又使用S32DS中的S32K118的例程程序进行编译烧录,提示出现附件图1的错误。使用Jflash connect,无法对芯片进行操作,不能烧写程序,也不能读取芯片内部信息。请问是否跟S32K118芯片内部起始地址有关。

0 Kudos
1 Solution
5,194 Views
Senlent
NXP TechSupport
NXP TechSupport

手里没有J-LINK调试器,要不然可以给你量一下,但是1.1V的应该是不对,5V供电的话,正常值应该在1.65~3.6之间

View solution in original post

0 Kudos
7 Replies
5,181 Views
Sally_Wang
Contributor I

再次确认,板子上的SWDIO引脚电压为1.1V左右,现截取SWD引脚的原理图,麻烦帮忙给出指导意见。仿真器上的接线是没有接错的。但是J-FLASH和J-LINK是无法识别到芯片。

0 Kudos
5,180 Views
Senlent
NXP TechSupport
NXP TechSupport

 

AN5426的参考方案,clk端口推荐是下拉的,我可以阅读下这个问的,然后再仔细检查下

Senlent_0-1669345010480.png

 

0 Kudos
5,190 Views
Sally_Wang
Contributor I

使用的是ARM V11的JTAG/SWD仿真器,SWDIO引脚的电压是1.1V,我现在截取了接口部分的原理图,麻烦帮忙指点一下,看下哪里出了问题。

0 Kudos
5,184 Views
Senlent
NXP TechSupport
NXP TechSupport

把DIO和CLK的两个上拉电阻去掉再试一下

0 Kudos
5,201 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi,

    这应该没关系,你这个调试器应该还没有连接成功,下载的时候是外部供电还是用调试器供电?我遇到出现图二的提示的时候通常出现在只使用J-LINK供电的情况下发生,  S32K11x系列只支持SWD,Segger的版本要求: J-Link V9.4及以上版本 + 软件J-Link V6.00d以上。

0 Kudos
5,198 Views
Sally_Wang
Contributor I
hi
非常感谢您的建议!板子上仿真器接口是板子上的外部电源供电,仿真器SWD接线正常,
J-LINK版本使用的是V6.98C,下载使用SWD,硬件接线正常,但是硬件上测量出SWDIO 和SWCLK两根对地电压有异常,分别是1.1V 3.8V请问正常吗?J-link command无法识别
0 Kudos
5,195 Views
Senlent
NXP TechSupport
NXP TechSupport

手里没有J-LINK调试器,要不然可以给你量一下,但是1.1V的应该是不对,5V供电的话,正常值应该在1.65~3.6之间

0 Kudos