"Extensions and Updates" and "Installation details"

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

"Extensions and Updates" and "Installation details"

598 次查看
Alan_Y
Contributor II

Hello,

I have already uninstalled RTD 2.0.2 in "Extensions and Updates", why RTD 2.0.2 still shows in "Installation details"? Is there any difference?

Alan_Y_0-1674114733170.png

Alan_Y_1-1674114753372.png

 

 

标记 (2)
0 项奖励
回复
2 回复数

590 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Alan,

After uninstalled RTD 2.0.2 in "Extensions and Updates", can you still see RTD 2.0.2 examples when click File->New->S32DS Project from Example? 

Have you tried to uninstall RTD 2.0.2 in "Installation details"?

If it still doesn't work, uninstalling S32DS and reinstalling may not be so much trouble.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

588 次查看
Alan_Y
Contributor II

Hi Robin,

After uninstalled RTD 2.0.2 in "Extensions and Updates", I can't see RTD 2.0.2 examples.

I haven't uninstall RTD 2.0.2 in "Installation details", and I don't know which is the right unistall method.

0 项奖励
回复