Hello I used s32k118 in my project and need to know what is the max number for writing in nvm and flash ?
Hi
Please find the information in "6.3.1.2 Reliability specifications" of S32K1xxDS.
Flex Memory Endurance Calculator is recommended. For more information about the EEPROM, please take a look at AN11983 Using the S32K1xx EEPROM Functionality.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------