i want linker file and startup file for S32K118 .

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i want linker file and startup file for S32K118 .

2,257件の閲覧回数
ibrahim_elaasy
Contributor II

i want linker file and startup file for S32K118 be compatible with MCAL SDK  .

i want to add my object files for certain section on Flash Memory and in RAM manually .

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,219件の閲覧回数
esser
Contributor I

Hello,

i didn't find the files (linker and startup)in the defined path when i downlaod the MCAL autosar for s32 k from NXP website 

 

0 件の賞賛
返信

2,025件の閲覧回数
frantisekdobes
NXP Employee
NXP Employee

The MCAL4.2 and MCAL4.3 releases contain sample application for S32K118 which includes startup and linker files. After you install the MCAL4.2 it is available here:
c:\NXP\AUTOSAR\S32K14X_MCAL4_2_RTM_1_0_1\S32K14X_MCAL4_2_RTM_1_0_1_Sample_Application\eclipse\plugins\IntegrationFramework_TS_T40D2M10I1R0\auxiliary\toolchains
Or if you use MCAL4.3 then it is available here:
c:\NXP\AUTOSAR\S32K14X_MCAL4_3_RTM_1_0_0\S32K14X_MCAL4_3_RTM_1_0_0_Sample_Application\eclipse\plugins\IntegrationFramework_TS_T40D2M10I0R0\auxiliary\toolchains

The MCAL4.0 release contains sample application for S32K144 only.


You could also take the linker and startup files from S32 Design Studio for ARM which is available for free from www.nxp.com. After you install S32DS the linker and startup files are available here (if installed to the default path):
c:\NXP\S32DS_ARM_v2018.R1\S32DS\S32SDK_S32K1xx_RTM_3.0.0\platform\devices\S32K118