g_pin_mux_InitConfigArr0 <__isr_vector> initialization issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

g_pin_mux_InitConfigArr0 <__isr_vector> initialization issue

568 Views
samcs
Contributor II

Hi NXP support team,

I debugged the project, set break point at rtos_start(), in function: int main(void),

the first line.

the global should be initialized, but used PEMicro, on Expressions window, I found: 

g_pin_mux_InitConfigArr0[73]
Details:{

base = 0x0 <__isr_vector>,

pinPortIdx = 0,

pullConfig = PORT_INTERNAL_PULL_NOT_ENABLED,

passiveFilter = false,

driveSelect = PORT_LOW_DRIVE_STRENGTH,

mux = PORT_PIN_DISABLED,

pinLock = false,

intConfig = PORT_DMA_INT_DISABLED,

clearIntFlag = false,

digitalFilter = false,

gpioBase = 0x0 <__isr_vector>,

direction = GPIO_INPUT_DIRECTION, initValue = 0 '\0'}

this will cause a the program stopped at default ISR.

I searched  pinPortIdx in pin_mux.c, got:

board
pin_mux.c (73 matches)
124: .pinPortIdx = 10U,

So the issue is only 73 items in g_pin_mux_InitConfigArr0[];

but in pin_mux.c,

 /* Generate array of configured pin structures */
pin_settings_config_t g_pin_mux_InitConfigArr0[NUM_OF_CONFIGURED_PINS0] = {

#define NUM_OF_CONFIGURED_PINS0 77 // in pin_mux.h,

i am wondering why the NUM_OF is 77 in pin_mux.h, 

I am using S32 Design Studio for S32 Platform Version: 3.4,S32K1XX SDK RTM 4.0.2.

Any help would be much appreciated.

 

 

 

0 Kudos
3 Replies

533 Views
danielmartynek
NXP TechSupport
NXP TechSupport
0 Kudos

550 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @samcs,

Can you please specify the MCU, IDE version and version of drivers?

Or can you share a test project that could reproduce it?

 

Thank you,

BR, Daniel

0 Kudos

545 Views
samcs
Contributor II

i found the reason, it's 4 pins be assigned to more functions, dual functions. 

I tried to remove a function,then update the code, for ex, PTA4 JTAG_TMS, SWD_DIO, 

set it to JTAT_TMS only, then update code, then the macro in pin_mux.h,NUM_OF_CONFIGURED_PINS0 be updated to 76.

but I don't know how to let the Macro only be number of pins, not number of pin functions.

0 Kudos