Unable to generate project in EB Tresos

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to generate project in EB Tresos

Jump to solution
753 Views
yash_bhatnagar9
Contributor II

Hi, I am unable to generate the project after importing the example project from "SW32K3_RTD_4.4_2.0.1" 1.png2.png3.png

After generating the project, the output folder remains empty. no config files are generated. Please provide some solution for this.

@mikedoidge  Please help

Tags (2)
0 Kudos
1 Solution
743 Views
nxf78987
NXP Employee
NXP Employee

Hi yash_bhatnagar9,

You can click right on the project's name and you can see that the config files were generated at the path below:

nxf78987_1-1661763758905.png

If you want to generate config files to the "output" folder => you can modify the generation path as the image below:

nxf78987_2-1661764051425.png

Best regards,

Dan

 

View solution in original post

1 Reply
744 Views
nxf78987
NXP Employee
NXP Employee

Hi yash_bhatnagar9,

You can click right on the project's name and you can see that the config files were generated at the path below:

nxf78987_1-1661763758905.png

If you want to generate config files to the "output" folder => you can modify the generation path as the image below:

nxf78987_2-1661764051425.png

Best regards,

Dan