Some questions about RTD version

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Some questions about RTD version

690 Views
Alan_Y
Contributor II

Hello,

I have some doubts about RTD version,

1. What's the difference between "Installation details" and "Extensions and Updates"?

2. I have already uninstalled RTD 2.0.2 in "Extensions and Updates", why RTD 2.0.2 still shows in "Installation details"? Is there any difference?

3. Should the development package "S32DS_3.4.1_D2110" and RTD package"

RTD_4.4_1.0.0_DS_updatesite_D2110" keep the same version? For example, should they both be D2110?

4. If I want to use both S32K344 and S32K342, which version of development package and RTD package should I use? Or I should use two versions of the packeges to fit K344 and K342 separately. If I should use two versions, can I install them in one IDE(S32 Design Studio 3.4.1)?

企业微信截图_1674025659279.png

企业微信截图_16740255976826.png

  

Tags (2)
0 Kudos
Reply
1 Reply

646 Views
mikedoidge
NXP Employee
NXP Employee

Hello,

The S32 Design Studio is a combination of the a base package of Eclipse with NXP-developed features and NXP-device specific support added on top. The S32DS Extensions and Updates is a feature of the S32 Design Studio. It was added to enable the ability to enforce dependencies between packages and to prevent incompatible installation configurations. The Installation Details and Install New Software features are part of the base Eclipse package which comes from the global Eclipse community. It is developed and maintained by the Eclipse community and is not modified by NXP.

The versions of the S32K3 development packages and S32K3 RTD AUTOSAR 4.4 packages are completely independent and any matches in version labeling are purely coincidental.

When you select the package in the S32DS Extensions and Updates feature, the Overview panel will detail which devices are supported by the package.

S32K3xx development package example:

mikedoidge_0-1678287320231.png

 

S32K3 RTD AUTOSAR 4.4 package example:

mikedoidge_1-1678287386718.png

I hope this helps!

Best Regards,

Mike

0 Kudos
Reply