Setting steps to change the trigger mode of ADC during program running

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Setting steps to change the trigger mode of ADC during program running

Jump to solution
893 Views
1090097669
Contributor III

Change the trigger mode of ADC1 during program running.

For example, during initialization,  ADC1 triggered by FTM3 via PDB1. After running to a specific condition, it needs to change from the previous trigger mode to the back-to-back mode of PDB1 to trigger ADC1。one of the two Running alone, I can achieve the purpose of triggering ADC1, but I can't switch between the two. If I change from FTM3 trigger to PDB1b back-to-back trigger, it will cause downtime. How to solve it?

0 Kudos
1 Solution
890 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello Katrinal,

Please take a look at the RM rev.12.1, Section 43.8 Trigger Selection.

There are two ways to change the triggering scheme but there will be always some downtime.

 

Regards,

Daniel

View solution in original post

0 Kudos
1 Reply
891 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello Katrinal,

Please take a look at the RM rev.12.1, Section 43.8 Trigger Selection.

There are two ways to change the triggering scheme but there will be always some downtime.

 

Regards,

Daniel

0 Kudos