S32K3X4EVB-T172 UART

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
654件の閲覧回数
jacob_ala
Contributor I

Hello! We're looking at testing with the S32K3X4EVB-T172 Evaluation Board for development of a custom automotive controller. How many UART peripherals are supported by this evaluation board?

Thank you!

0 件の賞賛
返信
1 解決策
640件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @jacob_ala 

As shown in the below image, S32K314, S32K324 and S32K344 has 15 UART instances. Also, you can refer to the S32K344_S32K324_S32K314_IOMUX.xlsx file attached to the RM to see the pins that can be configured for each UART. 

VaneB_0-1678828334819.png

 

B.R

VaneB

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
641件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @jacob_ala 

As shown in the below image, S32K314, S32K324 and S32K344 has 15 UART instances. Also, you can refer to the S32K344_S32K324_S32K314_IOMUX.xlsx file attached to the RM to see the pins that can be configured for each UART. 

VaneB_0-1678828334819.png

 

B.R

VaneB

 

0 件の賞賛
返信
637件の閲覧回数
jacob_ala
Contributor I
Perfect, thank you! As long as all those pins are accessible on the Evaluation Board, then it should work! Cheers
0 件の賞賛
返信