S32K3 Multilink(P&E) flash tool setting based on Design Studio 3.4.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K3 Multilink(P&E) flash tool setting based on Design Studio 3.4.

607件の閲覧回数
StephenYeh
Contributor III

Hi Sir

We based on the S32K3 to implement bootloader & application FW.

Is there any setting that the Design Studio(3.4) don't erase all the flash region?

Or we can set the erase area by the advanced options.(ex: The following options is mute. )

 

StephenYeh_0-1669276167611.png

 

タグ(1)
0 件の賞賛
返信
1 返信

592件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

There are 3 possible memory ranges that you can set to keep intact. It actually erases all the blocks, putting back what was originally stored at these locations, which is the same thing as a result.

davidtosenovjan_0-1669645266209.png

 

 

0 件の賞賛
返信