S32K148 chip, J-link can not connect after program disorder.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K148 chip, J-link can not connect after program disorder.

829件の閲覧回数
hjy1
Contributor I

Hello,

I have a issue with j-link debug.
My platform is S32K148, the debug tools is j-link, the 4 pin connect, GND-VCC-SWD-CLK.

But one time, I debug my code, maybe the program is not valid, the program run out of track, and pop up message.

pastedImage_1.png

From then on, the j-link can not connect with platform.

I have try below procedure

1. plug out power and plug in

The program can run part, but after part, disorder

2. make reset to low when connecting, also fail.

3. I have mark the SWD function when VLPS mode, I doubt the program have jump to VLPS.

For this issue, how to fix it, please help.

Thanks,

Fish.

タグ(1)
0 件の賞賛
返信
1 返信

782件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Fish,

Please refer the answer in: "error 7" using MSD flash programmer for s32k118evb

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信