S32K144EVB SPI Error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K144EVB SPI Error

818件の閲覧回数
kimmk
Contributor I

Hi,

I'm trying to use uja1169TK/F in S32K144EVM.

When operate SBC_SetCanConfig function, some error occured.

In SBC_SetCanConfig function -> SBC_DataTransfer->LPSPI_DRV_MasterTransferBlocking functions,

001.png

LPSPI_DRV_MasterTransferBlocking function is when SPI master transmits a data, SPI slave sends a data back to master at the same time.

But when that operated, receive failed.

002.PNG

This situation is same in lpspi_dma example, lpspi_transfer example.
how to solve this problem?

I upload this project.

0 件の賞賛
3 返答(返信)

810件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

How do you power the board?

The SCB requires 12V power supply.

Can you please scope the SPI bus?

 

Thank you,

BR, Daniel

0 件の賞賛

803件の閲覧回数
kimmk
Contributor I

Hi, Daniel,

 

I saw too many articles saying that 12V power should be input.

So, of course, it is inputting the power at 12V.

 

And below two picture attached.

first is when operate SBC_Init(), second is SBC_SetCanConfig.

Yellow = CS, Red = SCK, Blue = SDI, Green = SDO.

SBC_Init ScopeSBC_Init ScopeSBC_CanConfig ScopeSBC_CanConfig Scope

Best,

Minkyu.

0 件の賞賛

774件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello Minkyu,

I'm sorry for the delayed response.

I have tested the project and it works.

When the execution is halted after SBC_SetCanConfig(), I can see this:

danielmartynek_0-1613044060996.png

I only get the error that you reported while I'm stepping through the function.

 

Regards,

Daniel

0 件の賞賛