S32K144 interface voltage for ISELED

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K144 interface voltage for ISELED

Jump to solution
1,215 Views
nanjun
Contributor III

Hello,

the S32K144 is connected to iseledstrip through an adapter board.

The voltage from MCU is 3.3V while LED strip requires 5V. Could the MCU be damaged during read function?

See ISELED ADK User Manual.

Kind regards,

Neo

 

0 Kudos
1 Solution
1,200 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

when the supply voltage is 3.3V, the MCU is not 5V tolerant even if a pin is configured as open drain. The datasheet explicitly states that open drain pin must be pulled to VDD. And Vih spec says that input voltage can't exceed VDD+0.3V. If an external circuit requires 5V, the only options are either to use 5V supply voltage for MCU or use some voltage level translator.

Regards,

Lukas

View solution in original post

0 Kudos
2 Replies
1,201 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

when the supply voltage is 3.3V, the MCU is not 5V tolerant even if a pin is configured as open drain. The datasheet explicitly states that open drain pin must be pulled to VDD. And Vih spec says that input voltage can't exceed VDD+0.3V. If an external circuit requires 5V, the only options are either to use 5V supply voltage for MCU or use some voltage level translator.

Regards,

Lukas

0 Kudos
1,158 Views
nanjun
Contributor III

Hello Lucas,

thanks for your reply. Actualley I wrote you back some days before but it seems the email failed.

The problem was solved.

Kind regards,

Neo

 

 

0 Kudos