S32K144 XTAL no signal

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K144 XTAL no signal

423 Views
lengrudie
Contributor III

I use an external crystal oscillator and choose an external reference clock, but I use a signal generator to generate an 8M crystal oscillator input to the EXTAL pin, but I cannot measure the output waveform at the XTAL pin. EREFS=0 for SOSCFG.WHY?

0 Kudos
2 Replies

398 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @lengrudie 

The S32K1xx supports crystals or resonators from 4 MHz to 40 MHz.

Please refer to section 3.1 (EXTAL and XTAL pins) of the Hardware Design Guidelines for S32K1xx Microcontrollers, there are mentioned all the things you need to consider for the Quartz Crystal / Ceramic Resonator. 

 

B.R.

VaneB

0 Kudos

420 Views
lengrudie
Contributor III

To add, my configuration is as follows:SOSCCSR=0X0100,0001

SOSCDIV=0X0000,0101

SOSCCFG=0X0000,0030

0 Kudos