S32K144 Bootloader demo with PLL could not work

cancel
Showing results for 
Search instead for 
Did you mean: 

S32K144 Bootloader demo with PLL could not work

Jump to solution
629 Views
KILLERzheng
Contributor IV

I get the demo from unified bootloader framework, but it could not work with the PLL enable, and when the project init clock, it goes to hardware error. On the other hand, if I set the PLL false, it could works. I do not know where the error is. Besides the EXTAL of my board is 16MHz, is there any wrong with the hardware designing?

Tags (2)
0 Kudos
1 Solution
614 Views
Senlent
NXP Employee
NXP Employee

try this configuration.

Senlent_0-1644484549796.png

 

View solution in original post

0 Kudos
5 Replies
620 Views
Senlent
NXP Employee
NXP Employee

Hi@KILLERzheng

This routine uses an 8M external clock crystal oscillator by default. If you use a 16M crystal oscillator, there will be problems. You need to change the clock configuration, or replace the crystal oscillator with 8M. If you don't change the crystal oscillator, you have to change the configuration of the clock part of the BT and APP routines.

0 Kudos
616 Views
KILLERzheng
Contributor IV

Hi Senlent,

Thanks for you response.

I have not been familiar with PLL configuration, could you please give me some suggestions that how to configure with it?

0 Kudos
615 Views
Senlent
NXP Employee
NXP Employee

try this configuration.

Senlent_0-1644484549796.png

 

0 Kudos
608 Views
KILLERzheng
Contributor IV

Do you mean that way to modify the configuration?

 

KILLERzheng_0-1644485591003.png

 

0 Kudos
591 Views
Senlent
NXP Employee
NXP Employee

Hi@KILLERzheng

yes, please have a try.

0 Kudos