S32K116 LPIT high frequency interrupt
09-23-2019
09:40 AM
1,768 Views
rjmalmeida0
Contributor III
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi, i'm trying to toggle a pin at a frequency higher than 1MHz using the LPIT. I've configured the Sys, Bus and peripheral clock to the SOSC @ 40MHz configured frequency (as seen on printscreen). The issue appears when I try to configure the LPIT to interrupt every 40 ticks (or periods). The frequency of the pin toggle should be 1MHz but it goes down to 500kHz (approx). And when I put values lower than 40, the frequency slowly goes up from the 500kHz, at every lower value. Am I missing something? Below is my configuration inside main function and the ISR.
int main(void) {
/* Write your local variable definition here */
/* Initialize system and peripheral clocks */
CLOCK_SYS_Init(g_clockManConfigsArr, CLOCK_MANAGER_CONFIG_CNT,
g_clockManCallbacksArr, CLOCK_MANAGER_CALLBACK_CNT);
CLOCK_SYS_UpdateConfiguration(0U, CLOCK_MANAGER_POLICY_FORCIBLE);
/* Initialize Pin settings*/
PINS_DRV_Init(NUM_OF_CONFIGURED_PINS, g_pin_mux_InitConfigArr);
/* Install interrupt */
INT_SYS_InstallHandler(LPIT0_IRQn, &LPIT_ISR, (isr_t *) 0);
/* Enable interrupt */
INT_SYS_EnableIRQ(LPIT0_IRQn);
/* Initialize LPIT Timer */
LPIT_DRV_Init(INST_LPIT1, &lpit1_InitConfig);
LPIT_DRV_InitChannel(INST_LPIT1, 0U, &lpit1_ChnConfig0);
LPIT_DRV_StartTimerChannels(INST_LPIT1, (1 << 0U));
for (;;){}
return exit_code;
}
void LPIT_ISR(void)
{
PTB->PTOR = (((uint32_t)(((uint32_t)((1 << 13U)))<<GPIO_PTOR_PTTO_SHIFT))&GPIO_PTOR_PTTO_MASK);
/* Clear LPIT channel flag */
LPIT0->MSR = (1 << 0U);
}
Thanks in advance
1 Reply
09-30-2019
04:06 PM
1,464 Views
victorjimenez
NXP TechSupport
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello Rui,
Could you please share your project with me so I can reproduce the behavior you mentioned and make some tests on my side?
Best regards,
Victor