S32 can't find Hardware (S32K344) for Debug

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 can't find Hardware (S32K344) for Debug

Jump to solution
523 Views
Ojav
Contributor II

Hi guys,

i just finished the Getting Started Section for the S32K344 .

I installed "S32 Design Studio IDE", SDK and also the Real-Time Driver.

Using " ping 192.168.225.100 -t" works fine.

Next I wanted to follow the Getting Started with S32K3 using S32DS at the hello world project Training Presentation. 


Which worked fine until the debugging process. Where it cant detect my hardware.

I tried to use Ethernet as an Interface and also the J74 Type C Connector.

hardware.PNG

 

hardware2.PNG

Are there any Drivers I have to install? My Device Manager doesnt update if I plug the USB-C in.

Ojav_0-1678696804263.png

 

What are the steps so my S32 Studio can detect my S32K344 Device?

 

EDIT1: To be clear I don't have a PEmicro JTAG connector connected. Is there no Onboard debugging connection?

0 Kudos
1 Solution
502 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @Ojav,

The S32K344 MCU can be reprogrammed via the J40 JTAG/SWD connector only.

There is no on-board programmer/debugger.

 

Regards,

Daniel

 

View solution in original post

1 Reply
503 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @Ojav,

The S32K344 MCU can be reprogrammed via the J40 JTAG/SWD connector only.

There is no on-board programmer/debugger.

 

Regards,

Daniel