S32 Design studio V3.4 installation unsuccessful and roll back

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32 Design studio V3.4 installation unsuccessful and roll back

跳至解决方案
797 次查看
WeiboQiu
NXP Employee
NXP Employee

I have initiated Administrator access and copied the license received by email. I chose online as I have internet connected.  However, I still face the installation failure. when it arrives at 6% of the installation, it rolls back and said installation unsuccessful. I traced the log and see blow:

Install Uninstaller: S32 Design Studio for S32 Platform 3.4(Install All Uninstaller Components)
Status: ERROR
Additional Notes: ERROR - Error writing LaunchAnywhere components (Access Denied)

 

0 项奖励
回复
1 解答
788 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi WeiboQiu,

For NXP Employee, please refer to the discussion here: After retry to install S32DS_3.5.0 few times, the software failed everytime

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
789 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi WeiboQiu,

For NXP Employee, please refer to the discussion here: After retry to install S32DS_3.5.0 few times, the software failed everytime

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复
782 次查看
WeiboQiu
NXP Employee
NXP Employee

Hi,

Thanks for your reply. the solution you posted is for S32 design studio v3.5, but also worked in my case for S32 design studio v3.4

0 项奖励
回复