PFS26ZZXMA0D on S32K3X4EVB-Q172

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

PFS26ZZXMA0D on S32K3X4EVB-Q172

跳至解决方案
1,567 次查看
20Sidar04
Contributor III

Dear Mr. and Mrs.,

is PFS26ZZXMA0D ASIL B or ASILD on S32K3X4EVB-Q172?

Best Regards,

Sidar

1 解答
1,548 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Sidar,

It is the PFS2613AMDA2AD used on an S32K3x4EVB-Q172 board. This part has been updated to Production part number: MFS2613AMDA2AD. So it is ASIL D variant.

BR, Tomas

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,549 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Sidar,

It is the PFS2613AMDA2AD used on an S32K3x4EVB-Q172 board. This part has been updated to Production part number: MFS2613AMDA2AD. So it is ASIL D variant.

BR, Tomas

0 项奖励
回复
298 次查看
fortannekita
Contributor I

I don't think it is MFS2613AMDA2AD. Here's the OTP config for MFS2613AMDA2AD.
While on evaluation board VPRE is 5.5V, LDO1 is 3.3V, LDO2 is 5V and VREF 3.3V

fortannekita_0-1735051203510.png

 

0 项奖励
回复
1,545 次查看
20Sidar04
Contributor III

Hello Tomas,

Thanks for response. What is difference between PFS2613AMDA2AD and MFS2613AMDA2AD.

Regards.

0 项奖励
回复