PFS26ZZXMA0D on S32K3X4EVB-Q172

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PFS26ZZXMA0D on S32K3X4EVB-Q172

ソリューションへジャンプ
1,564件の閲覧回数
20Sidar04
Contributor III

Dear Mr. and Mrs.,

is PFS26ZZXMA0D ASIL B or ASILD on S32K3X4EVB-Q172?

Best Regards,

Sidar

1 解決策
1,545件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Sidar,

It is the PFS2613AMDA2AD used on an S32K3x4EVB-Q172 board. This part has been updated to Production part number: MFS2613AMDA2AD. So it is ASIL D variant.

BR, Tomas

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,546件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Sidar,

It is the PFS2613AMDA2AD used on an S32K3x4EVB-Q172 board. This part has been updated to Production part number: MFS2613AMDA2AD. So it is ASIL D variant.

BR, Tomas

0 件の賞賛
返信
295件の閲覧回数
fortannekita
Contributor I

I don't think it is MFS2613AMDA2AD. Here's the OTP config for MFS2613AMDA2AD.
While on evaluation board VPRE is 5.5V, LDO1 is 3.3V, LDO2 is 5V and VREF 3.3V

fortannekita_0-1735051203510.png

 

0 件の賞賛
返信
1,542件の閲覧回数
20Sidar04
Contributor III

Hello Tomas,

Thanks for response. What is difference between PFS2613AMDA2AD and MFS2613AMDA2AD.

Regards.

0 件の賞賛
返信