MC33772B sleep cmd not work

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC33772B sleep cmd not work

1,933 Views
dadaoyiyang
Contributor I

working on BSM system: s32k148    <-spi->   MC33772BSP2AE

communication and cells measurement works now,

trying to set MC33772B go to sleep mode, Spi write cmd such as

0x0, 0x1, 0x2, 0x1E, 0x5A, got feedback 0xFF, 0xFF, 0xFF, 0xFF, 0xFF,

sleep cmd not executed. 

before this sleep cmd , previous read/write spi cmd all correct executed.

Do you know under which condition an all 0xFF feedback would replayed. 

and any other action should be executed before send sleep CMD?

 

 

 

0 Kudos
5 Replies

1,883 Views
dadaoyiyang
Contributor I

Hi, 

           The datasheet I checked is  "MC33772B Battery cell controller IC Rev. 6.0 — 2 April 2020 "   as the chip we used is MC33772B, 

      thanks for your information, I will do some other test , then give you feedback.

Thanks!

0 Kudos

1,876 Views
reyes
NXP TechSupport
NXP TechSupport

Hi,

Thanks for the correction, sorry about that.

On the MC33772B, under SPI communication, a local write command is necessary just as mentioned for the MC33772C. however, different from the MC33772C, the MC33772B, upon receipt of a "go to sleep" command, if the IC is being performing a conversion sequence, then the state transition is delayed until an EOC occurs (end of conversion); else, the state transition occurs immediately. In other words, the device goes to sleep mode only after all conversions in progress are completed.

 

If you check the attached state diagram image for the MC33772B, to go from normal mode to sleep mode, it is not only required to set SYS_CFG_GLOBAL[GO2SLEEP] bit to logic 1, but also EOC should occur (end of conversion).

reyes_0-1629132638363.png

 

Regards,

Jose

0 Kudos

1,923 Views
reyes
NXP TechSupport
NXP TechSupport

Hi,

To instruct the MC33772C to enter the Sleep mode, the user sets the SYS_CFG_GLOBAL[GO2SLEEP] bit to logic 1. If the communication type is TPL, only a global write command can be used, while in case of pure SPI communication, a local write command is necessary

 

I’m not sure why you got feedback when writing to the registers since, unlike the read command, for which MC33772C responds with data, the write command does not generate any response. When the slave receives a valid LOCAL WRITE COMMAND, the message is acted upon but no response is generated.

 

Regards,

Jose

0 Kudos

1,920 Views
dadaoyiyang
Contributor I

Hi Jose,

              Thanks for your feedback!

              the "response" may not correct, actually it's the echo of write command,

       in datasheet,

10.4.2 Write local command
Unlike the read command, which responds with data, the 33772 responds to the write
command with a single frame echo of the command and updated register contents.

a successful write cmd   with correct echo

AFE_Tx = (0x0, 0x0, 0x26, 0x12, 0x20)
AFE_Rx = (0x0, 0x0, 0xA6, 0x12, 0x27)

but when trying to write SYS_CFG_GLOBAL[GO2SLEEP] bit to logic 1,got  all 0xFF echo, and sleep not executed.

AFE_Tx = (0x0, 0x1, 0x2, 0x16, 0x0D)
AFE_Rx = (0xFF, 0xFF, 0xFF, 0xFF, 0xFF)

 

before this sleep cmd , I wrote three register : FAULT1_STATUS,FAULT2_STATUS,FAULT3_STATUS

all with correct echo returned.

so is there any precondition to write SYS_CFG_GLOBAL[GO2SLEEP] bit to logic 1?

 

Thanks!

0 Kudos

1,915 Views
reyes
NXP TechSupport
NXP TechSupport

Hi,

Can I ask which version of the datasheet are you looking?

I’m looking into the version Rev. 3 — 4 June 2021 of the MC33772C (can be downloaded from NXP DocStore) where section 10.4.2 ‘Local Write Command’ specifies:

“Unlike the read command, for which MC33772C responds with data, the write command

does not generate any response. When the slave receives a valid local write command,

the message is acted upon but no response is generated”

And tables of this section (image below) doesn’t specify anything about an echo response.

reyes_0-1628868430912.png

 

There are no preconditions to write SYS_CFG_GLOBAL[GO2SLEEP] bit to logic 1, this should be straight forward and the MC33772C should go into sleep mode when setting this bit. As you can see in the  state diagram image below, to go from normal mode to sleep mode, the only requirement is to set SYS_CFG_GLOBAL[GO2SLEEP] bit to logic 1.

reyes_1-1628868476152.png

 

Regards,

Jose

0 Kudos